Description Some users may desire to record a different resolution or frame rate from a camera when an event such as motion or an analytic is triggered. Reasons for this vary by site, but often comes down to wishing to record a lower amount of data when very little is happening, but they require high… Continue reading Recording different resolution or frame rates on event
Tag: Lower Frame Rates
Lower Frame Rates Displayed than Expected
At times, the number of frames per second displayed on an exacqVision system might be lower than expected. This can be caused by network bandwidth, the processor, or the display driver. To determine the cause of the issue, click the kB/s indicator in the exacqVision Client status bar multiple times to cycle through the following… Continue reading Lower Frame Rates Displayed than Expected