Problem
In lower light conditions motion may be triggered constantly or not at all. This can be seen in the camera webpage as well where the last motion alarm is a start alarm followed by no stop.
Solution
To reduce the false triggers the following can be done.
- Reduce the sensitivity of the motion area.
- Draw multiple motion windows in the area.
- Reduce the sharpness of the image. (This may make the image slightly blurry).
You should now see start and stop alarms in the camera web page as well as recording in exacq.