Starting with server version 19.08, it is now possible to collect additional information about storage self tests. evselftestYYYY-MM-DD.txt files in the server/logs path will trace all of the commands that evselftest issues along with their corresponding output. This feature is turned on when the EvselftestLogEnabled attribute under “Storage” is set to “1” in sysmgmtpi.xml.