For Ubuntu, adding a new locale (language) is a two-step process. First, determine the UTF8-encoded locale name, then generate the UTF8-encoded locale. <br> Determine Locale Name Open a command line window and type: less /user/share/i18n/SUPPORTED This will list all of the locales Ubuntu supports. Scroll down to find the one that matches the ISO 639-1/ISO… Continue reading Adding/Configuring Locales on Ubuntu Linux