Installing 32-bit Enterprise Manager (EM) on 64-bit 14.04 or 16.04 Ubuntu Linux System

Objective Installing 32-bit Enterprise Manager on a 64-bit Ubuntu 14.04 or 16.04 Linux computer, complete the following steps: <br> Instructions Configuring a new system. <br> Setup multiarch <br> Remote Setup Ensure that X Windows can be forwarded to anyone using Putty or SSH (install gedit).Use Filezilla to transfer the debian installer to the instance.Connect using… Continue reading Installing 32-bit Enterprise Manager (EM) on 64-bit 14.04 or 16.04 Ubuntu Linux System

Moving an eDVR Board in a Linux System

The following steps should be followed when moving the eDVR boards: In the exacqVision Client, save the system settings and note the serial number associated with the eDVR boards in the tree order by clicking on the board icons in the Configuration tree.Shut down the system.Unscrew the boards from the existing mounting. Do not disconnect… Continue reading Moving an eDVR Board in a Linux System