Skip to content

Exacq

Support Portal CMS

Tag: Linux doesn’t remove dynamically assigned IP addresses

Linux Doesn’t Remove Dynamically Assigned IP Addresses When NIC Unplugged

Description Linux doesn’t drop network configuration when a dynamically-assigned NIC is unplugged as Windows does. However, if the package ifplugd is installed then it will.

Published May 4, 2021
Categorized as Knowledge Support, Support, Categories, Products, exacqVision Integrations Tagged Level2, NIC Unplugged, Linux doesn’t remove dynamically assigned IP addresses, IP Addresses, 5199

Recent Posts

  • Synchronize with Enterprise Manager authentication – Connectivity error:500
  • Exacq Mobile Application Views show Black Box
  • Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
  • FLIR Camera Motion Stops Recording Motion Events
  • exacqVision 25H1 Release Bulletin