Archiving Stalls on Linux-based exacqVision Systems

Archiving from a Linux-based exacqVision system over a wide-area network (WAN) can stall in a Writing Files status for over an hour. If you believe a system is affected, verify the following conditions and symptoms: Linux kernel version 3.0 or later. Previous versions are not believed to be affected. (To determine the kernel version, run uname… Continue reading Archiving Stalls on Linux-based exacqVision Systems