Description Illustra3 supports a separate http socket to stream metadata such as analytic/motion/input trigger. This allows the device level support of events independent of the video stream. Which provides a device level connection state that could be use to monitor the device. <br> Version Introduced r52213 (RC 5.10.x) <br> Platform All <br> Steps to reproduce illustra3… Continue reading Illustra3 links device level connection to video stream