Legacy Arecont Camera Frame Rates

Description  Arecont Legacy cameras are limited to the amount of Frames Per Second they send when using Full Resolution vs Half Resolution.Example of Cameras:Arecont AV12176DN-NLArecont AV2455DN-FArecont AV5555DN-S Product  If you find that the Received Frames Per Second or Decoded Frames Per Second are Half the FPS it is due to the limitations of the cameras… Continue reading Legacy Arecont Camera Frame Rates

Cloudvue Legacy Subscription Accounts

Description Cloudvue GatewayC2C Solution Service Plan – TCSVMSM – VMS only Monthly Storage Retention – No Cloud Drive Legacy Accounts Account1800Packouts7thGenAccess Control ConsultantsAces LLCACS, JOCO LibraryAcurixAmerisureAndani ImportsApple Security SolutionsArbelbide Farms LLCBagby and RussellBally RibbonBeltoneNEBridgewayBrite StarBuilders TrustCE PizzaClaresholmCoastal PizzaDawg ParadiseDesert HillsDuke CommunicationsElauwitElauwit, EdREmpiretecheSecurity, Wash N RollFidelis SolutionsFloors DirectFuller Apt HomesHightekInnovative ITisoflexITZ NetworksJCSSJetz FoodsJohnson Controls Inc, Sammamish… Continue reading Cloudvue Legacy Subscription Accounts

Creating a Self-Signed SSL Certificate

Before Beginning… Requirements You will need the OpenSSL program to create a self-signed certificate. The method of obtaining this program varies based on the operating system used. Note: A certificate generated on either platform will work on the other (i.e.- a certificate generated using openssl on Linux can be used with a Windows web service).… Continue reading Creating a Self-Signed SSL Certificate

Replacing a Drive in Ubuntu 20.04 or later, Using GParted (Legacy)

This procedure is applicable to replacing the primary hard drive of a Linux-based exacqVision system. It assumes that the operating device is installed to an on-board flash device. Do NOT use this procedure when simply adding a drive to a system.

Firefox – Updating Old Ubuntu Repositories

Title Firefox – Updating Old Ubuntu Repositories Description  Once an Ubuntu release has hit it’s end of life (EOL) date it may be necessary to manually add sources to the repository sources.list in order to update Firefox to a version that will have meet the minimum requirements to work with modern websites and software.  Product … Continue reading Firefox – Updating Old Ubuntu Repositories

exacqVision Legacy Software Downloads

Title exacqVision Legacy Software Downloads    Description Legacy versions of exacqVision software too include 32-bit, 64-bit, Linux, MacOS, Windows, and Window MSI are available for download.     Product  exacqVision Client exacqVision Server Edge M-Series exacqVision Web Service exacqVision Enterprise Manager   Solution   Older versions of exacqVision Server and Client software are available on our… Continue reading exacqVision Legacy Software Downloads

Dewarping of Dahua cameras not working on web client or Exacq Mobile 3 (Legacy)

Affected Versions <br> Description In web service 7.6 (Windows only), dewarping of Dahua fisheye cameras does not work. These cameras do not show any dewarping options in the web client or Exacq Mobile 3 app. <br> Workaround <br> Resolution Update exacqVision Web Service to version 8.2.2 or higher <br>

Enabling Legacy Authentication Mode

*** INTERNAL USE *** With the introduction of the new Authentication mode in exacqVision Client and Server 6.8, the temporary admin password no longer works. However, exacqVision Client includes a way to run in Legacy mode, thus enabling the temporary admin password. <br> This procedure should be used only by Exacq Technical Support. Double-click on… Continue reading Enabling Legacy Authentication Mode