Affected platforms exacqVision 6.4 or higher <br> Symptom Every time there is a config or alarm event from core, the IP camera detect plugin (IPCamDetectPI.dll) will leak memory. The memory leak is in small increments and on systems where huge number of events are happening, like lots and lots of motion events for example, the… Continue reading Camera discovery plugin leaks memory
Tag: Leak
Internal memory leak when sending email
Affected platforms exacqVision 4.12.3 to 7.0 <br> Symptom There is a small memory leak whenever the server executes a program. This leak is unlikely to cause a problem on any desktop systems, but it could cause a hang or reboot on Edge systems with limited memory, if the Edge server is configured to send frequent… Continue reading Internal memory leak when sending email
Exacqd handle leak
Symptom: It is possible after a very long period for the server to stop functioning, requiring a restart. Problem: There is a slow handle leak in exacqd introduced in server version 9.5.25/9.6.0. This handle is never used, so a slow memory leak is the result. Windows has a limit of 16 million handles. A server… Continue reading Exacqd handle leak