Issue Customers using exacqVision LC Series IP servers with H110M motherboards need to upgrade to Ubuntu 18.04 to avoid an issue in which the client could freeze the system. <br> Resolution Model Number and Motherboard information can be found in the System Information section on the System tab. (Configuration > YOUR SYSTEM NAME > Configure… Continue reading LC Series IP Servers with H-110M Motherboards Freezing