Description On a customer site, we have seen high CPU utilization in the 85% or more range with multiple cores (more than 20 cores). ESM will spin up a sub importer per core, so there could be 20+ sub importers in this scenario. Each using CPU, the total can be very high. On newer windows… Continue reading High CPU utilization for large ESM deploys on server 2008 in windows