Technical Bulletin – TAB Number: TB-00456-00-241004 Date Issued: 4th October 2024 Issue Required language is not included in list of pre-installed languages. Solution Add a language to the list of preferred windows display languages. Procedure: <br> Continuous improvement statement As with all processes defined by the Exacq Technical Services Group, this document is intended to… Continue reading Technical Bulletin: Installing Additional Languages for Windows 11
Tag: Language
Adding/Configuring Locales on Ubuntu Linux
For Ubuntu, adding a new locale (language) is a two-step process. First, determine the UTF8-encoded locale name, then generate the UTF8-encoded locale. <br> Determine Locale Name Open a command line window and type: less /user/share/i18n/SUPPORTED This will list all of the locales Ubuntu supports. Scroll down to find the one that matches the ISO 639-1/ISO… Continue reading Adding/Configuring Locales on Ubuntu Linux