Using exacqVision Web Service with Edge Cameras

Edge cameras cannot run the exacqVision Web Service. If you want to connect to an Edge camera using the Web Client or the Exacq Mobile 3 app you will need to install the exacqVision Web Service on another machine. The web service can be run on other machines but you will need to enter the… Continue reading Using exacqVision Web Service with Edge Cameras

Updating LAN Firmware on exacqVision Systems with Intel 82574L & 82579LM Network Adapters

A small percentage of exacqVision systems with Intel 82574L and 82579LM network adapters have been found to exhibit widely fluctuating network performance and then lock up. The problem can be resolved by updating the adapter firmware. To determine whether your system contain these adapters and require the update, follow the following process appropriate for your… Continue reading Updating LAN Firmware on exacqVision Systems with Intel 82574L & 82579LM Network Adapters