Q Series Units Using KVM Switch Showing No Display on Boot Up and when switching between units.

This is for a specific customer that was reporting issues with Q series units using a KMV Startech Switch-Model SV431USB.The customer experiences NO DISPLAY on the monitor on boot. They also exhibit no display when switching the source at the switch from a windows based unit back to the Q Series. Tickets: 22721 and 23035.… Continue reading Q Series Units Using KVM Switch Showing No Display on Boot Up and when switching between units.