ESM: Known database errors.

ESM displays an error in its log files indicating one of the following database related errors: ProgrammingError…DatabaseError…OperationalError…InterfaceError… This is expected behavior if the log message shows it was caught by !RunDatabaseQuery and also logs that the query recovered without exception.  This is an example of an error communicating with the database but has recovered. [16/Jun/2016… Continue reading ESM: Known database errors.