This document will guide you through step-by-step procedures for keyboard use and suggested button mappings. Product The Axis TU9001 Control Board consists of the combination of the TU9002 Joystick and the TU9003 Keypad. IMPORTANT: The TU9002 and TU9003 appear to the operating system as separate devices. As of Client version 24.03 only one Joystick device… Continue reading Using the Axis TU9001 Control Board with exacqVision
Tag: Joystick
Joystick
Use the Joystick configuration page to calibrate a new joystick or exacqVision Surveillance Keyboard, and assign button actions. Learn how to navigate and perform actions with the joystick in Live mode.
Using the ADVCPTZKEY1 USB Joystick / Keyboard with exacqVision
This document will guide you through step-by-step procedures for keyboard use and suggested button mappings. Prerequisites For proper operation of the American Dynamics ADVCPTZKEY1 PTZ USB Keyboard, both the exacqVision Client and Server must be on version 22.03 or higher. Product ADVCPTZKEY1 American Dynamics Surveillance Keyboard <br> Setup <br>
Joystick Z-Axis on Mac-based exacqVision Client
When using a joystick on Mac-based exacqVision Client software, Z-Axis operations do not work correctly. On an exacqVision Surveillance Keyboard (and most other devices), the joystick’s Z-Axis is mapped to the action of twisting the joystick, which is used to control zoom functions. On some keyboards, zoom functionality can be mapped to a programmable button.… Continue reading Joystick Z-Axis on Mac-based exacqVision Client
Can I use a Joystick with exacqVision Client software instead of a mouse?
Yes. Exacq offers the exacqVision Surveillance Keyboard for this purpose. <br>