Enterprise Manager Updating Java Version in Solr

Issue Enterprise Manager uses a package called Solr which in turn uses Java.  Currently, we do not offer an update path for Solr that will update the Java version.  The following instructions can be used if the need arises were Java needs to be updated.   Resolution Windows 64-bit Assumes EM is installed at C:\program files\exacqVision\EnterpriseManager for Windows 64 bitDownload… Continue reading Enterprise Manager Updating Java Version in Solr