An iSCSI configuration could be corrupt if the following are true: Linux-based exacqVision ServeriSCSI used as extended storageExtended Storage portal status displayed in exacqVision Client as anything other than OKServer logs contain the following messages:8/21/2014 1:48:12 PM ArchivePI Warning Errors from /usr/local/exacq/server/scripts/iscsiprep.py addportal -portaladdr 10.16.1.106 -portalport 32608/21/2014 1:48:12 PM ArchivePI Warning Error: while running command… Continue reading Troubleshooting a Corrupt iSCSI Configuration