The standard form for exacqVision camera addresses is as follows: {host}{?parameter_1=value_1}…{?parameter_n=value_n}{#override_1=value_1}…{#override_n=value_n} <br><br> Overrides PluginOptionUsageACTitransport=httpHTTP stream support for legacy platforms and user dataACTitransport=rtspRTSP stream with separate metadata socket for motion/input trigger/video loss/etc.Axiszoom=configBy default zoom only cameras support.Axiszoom=operationForce zoom only operation and controls as part of PTZ and live view.Axisblocksize=offOn by default, but could turn off blocksize… Continue reading IP Plugin Overrides
Tag: IQEye
Using IQeye Input Triggers
When a digital input is triggered on an IQeye camera, the camera transmits a single alarm to indicate the condition. This means that the triggered state cannot be seen on exacqVision Client’s Trigger Input page. To test IQeye digital inputs, you must use them with Event Linking or Event Monitoring. <br>
IQEye and Arecont Settings Not Changing
When you adjust settings for certain Arecont or IQEye cameras using the exacqVision Client, the settings do not get applied. If this occurs, see the following information for each camera brand. <br> Arecont There are no standard credentials for an Arecont camera, but with some models you can enter anything in the credentials area on… Continue reading IQEye and Arecont Settings Not Changing