Setting up Email Notifications to send a Start and a Stop email when the event starts and ends.

When setting up email notifications to work with a IP Camera Connection event there is setting in the Notifications to send on the event start and end. Once the Email Profile has been tested and confirmed to be working we need to set up 2 rules for this to work properly Event Linking To set… Continue reading Setting up Email Notifications to send a Start and a Stop email when the event starts and ends.

Differences Between Device and Audio Connection Alarms and IP Camera Connection Alarms

IP CONNECTION ALARMS Available in client under Event Linking and/or Event Monitoring under source type IP Camera Connection and video source’s name as configured under Camera Settings. It is always helpful to give your cameras unique, easily-recognizable names.Each stream is an independent alarm source, whether an encoder with multiple channels, or an IP camera with multiple active… Continue reading Differences Between Device and Audio Connection Alarms and IP Camera Connection Alarms