Exacq Mobile 3 Unable to Connect on iOS

Issue Exacq Mobile 3, version 20.06, has additional restrictions for service connections on iOS.  Apple recently deprecated UIWebView in favor of WKWebView requiring an update to the exacqVision Mobile to use WKWebView.  One of these restrictions is the requirement of CORS support for all requests.  The web service does not include these headers when performing a HTTP ->… Continue reading Exacq Mobile 3 Unable to Connect on iOS