iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution

Description iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution <br> Summary iOS Application crashes when decoding H.264 video from some axis sources in 800×450 resolution. This has been seen on a customers M5014 with firmware 5.25.2 as well as an M5014 with firmware 5.40.11.2 at the Exacq Fishers office. <br>… Continue reading iOS Application crashes when decoding H.264 video from Axis M5014 in 800×450 resolution