Symptom:
Connection to Panasonic device is stuck in “Connecting” despite displaying the model and MAC address.
<br>
Problem:
The following Panasonic devices were found to return an invalid image size when using firmware 1.03 or 1.10.
- WV-S1550L
- WV-S2131L
- WV-S2250L
- WV-S2550L
- WV-S8530N
- WV-X8570N
<br>
Solution:
Panasonic is planning to release a firmware update to address this issue.
<br>
Unable-to-Connect-to-Panasonic-Device-with-FW-1.03-or-1.10-2.pdf