Description Rtsp_lib is a layer of code that interface with Live555 for streaming video/audio/metadata and the camera plugins Axis/Dahua(essentials)/illusta3/illustraFlex/Hikvision(e-series)/Samsung/Panasonic/Sony/IQEye/UDP/RTSP/Pelco). We have seen an issue with Pelco Optera and IllustraFlexcameras that emit either larger than allocated userdata or 0 length sps packets and caused the server to crash. This is not very common but need to… Continue reading RTSP library crashes with invalid h264 packet from camera