When a Panasonic camera is configured for Internet mode (over HTTP) when using H.264 or MPEG-4 compression, the camera’s trigger inputs do not work correctly. The triggers are in a normally open state by default, but they do not enter an alarm state when the circuit is closed. <br>