Description As a result of KB https://support.exacq.com/#/knowledge-base/article/5610 the C1410 MK II can not alone create event linking to trigger through Exacq software. Exacq currently does not support the use of webhooks seen in the above KB. This guide will assist you with configuring an Axis D3110 Connectivity Hub to trigger the C1410 MK II via… Continue reading Using an Axis D3110 Connectivity Hub with the Axis C1410 MK11 Speaker
Tag: Internal
Configuring RTSP Streams in exacqVision Client
Note: This is an INTERNAL document – please do not share. VLC Configuration Add the RTSP Stream to exacqVision Client
Internal Test
This is an Internal test document – please ignore.