Using the Axis I8116-E Network Video Intercom with ExacqVision

This article applies to the Axis I8116-E Network Video Intercom using firmware 11.8.66. ExacqVision does not currently support SIP calling functions. However, this device can be integrated for interactive operation with ExacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the door station call button brings… Continue reading Using the Axis I8116-E Network Video Intercom with ExacqVision

Using the Axis A8207 Door Station with exacqVision

This article applies to the Axis A8207-VE and A8207-VE MkII Network Video Door Stations using firmware 11.5.64. exacqVision does not currently support SIP calling functions. However, these door stations can be integrated for interactive operation with exacqVision as detailed here. In the example that follows we will step through an example scenario wherein pressing the… Continue reading Using the Axis A8207 Door Station with exacqVision

Live Chat – Overview

Live Chats Live chats are being introduced to provide our customers “users” another method to quickly access technical support.  It provides a more rigorous and regimented vetting process, quickly guiding users to the information they need before requiring the assistance of a Live Chat operator. An automated Bot will guide Users through a series of… Continue reading Live Chat – Overview

Live Chat – Access and Settings

Title Live Chat – Access and Settings Description  This Knowledge Base Article contains information regarding the recommended intercom account settings for Exacq Live Chat operators. Accessing Intercom https://app.intercom.com Note:  You should have received an invite to initially setup an account, if not please contact your manager. Intercom Support Forum For answers to questions and information… Continue reading Live Chat – Access and Settings