Description Axis thermal cameras provide heat-based detection for monitoring property or detecting thermal anomalies which could lead to incidents involving smoke or fire. This guide is intended to introduce the use of these devices with your exacqVision VMS software. Requirements At the time of writing this article, these instructions pertain to the Axis Q19 Series… Continue reading Axis Q19 Series Thermal Cameras Integration Guide
Tag: Integration Guide
exacqVision DSX Integration Guide
Overview DSX is a powerful access control system monitoring application. This integration solely supports PTZ, Live View and Recorded View video and utilizes evAPI. <br> Requirements <br> Installation Before configuring WinDSX for use with the exacqVision System, complete the following steps: <br> Configuration <br> <br> <br> <br> <br> NOTE: If socket errors appear when you… Continue reading exacqVision DSX Integration Guide
Road AI LPR application with Hanwha Cameras
Overview Hanwha cameras may be configured with the Road AI license plate recognition application. The data from license plate captures can be viewed in the ExacqVision Client as text, sent as serial data over IP. The Road AI application is pre-installed and licensed from the factory on select camera models. This document will step through… Continue reading Road AI LPR application with Hanwha Cameras
Axis D2110-VE Security Radar Integration Guide
Adding a Louroe Digifact IP Microphone to ExacqVision Server
Title Adding a Louroe Digifact IP Microphone to ExacqVision Server Description How to integrate with a Louroe Digifact IP audio device to your ExacqVision Server. Product Solution Refer to the following integration guide.