Description As soon as you enable (check the Bosh integration profile . the system will reboot the exacq server service. Product Server Version 20.03 up to 22.12 were experiencing this crash. Panel in use: Bosch B9512GT Steps to Reproduce Configure the Add Security Integrations Page in the Client Select the Enable buttonThe server would lock… Continue reading Bosch Security Integration Causing Operating System to Crash
Tag: Integration Fails
First command to unlock/lock door or other action via Kantech integration fails
Affected platforms exacqVision Server 7.2.0 <br> Symptom When sending a command to an access control module (lock/unlock door, activate/deactivate relays etc.) the first attempt may fail silently. This is likely to happen if the operator credentials are same as the connection credentials. All subsequent commands will succeed or fail with an error message. <br> Workaround… Continue reading First command to unlock/lock door or other action via Kantech integration fails