Description Traditionally Cloudvue has focused on individual API integrations for cameras connecting to the Cloudvue Gateway. However, there are just too many camera manufactures to integrate with each. So, except for Illustra and Axis we rely on integrating with ONVIF Profile-S compliant cameras. Customers that would like a specific API camera integration should submit their… Continue reading Cloudvue Gateway Camera Integrations
Tag: Integration
exacqVision S2 OVID Driver for Linux Fails to Install
Description The exacqVisionOVID.deb file available at https://exacq.com/reseller/exacqVisionOVID.deb fails to install on both Ubuntu Linux 18.04 and 20.04. Product Steps to Reproduce Expected Results The OVID package installs successfully Actual Results The install fails with the following error. Solution Run the following commands. NOTE: ./cfgedit still fails to work but caja can be used to edit ovid.ini See trac Ticket #23269 for… Continue reading exacqVision S2 OVID Driver for Linux Fails to Install
Lenel Onguard Displays Yellow X Instead of Live Video
Issue Within Lenel Onguard software, a yellow X is being displayed instead of live video. This was being caused when trailing spaces were present in the camera names within exacq. Solution Cameras should now display video as expected
C-Cure Integration License
In order to fully integrate with C-Cure 9000 Versions 2.80 or later an additional license is required. The license can be requested from the CCURE’s licensing system via part number CC9WS-EXACQMON. After proper application, this license will show up in the CCURE “Licensing” application as “Exacq Analytics for CCURE 9000”. Here is an example:
Changes made to Entrapass connection parameters in exacqVision client are ignored
Affected platforms exacqVision Server 7.2.0 <br> Symptom Once successfully connected to an Entrapass server, changes to any connection parameters (IP address, port, username, password) are ignored. The connection will continue to attempt connection using the prior settings. <br> Workaround Dsiable the existing connection and create a new connection with new parameters. <br> Resolution Update to… Continue reading Changes made to Entrapass connection parameters in exacqVision client are ignored