Categories
Knowledge Support Support Categories Products exacqVision Integrations

Integrating exacqVision with a Kantech EntraPass installation that uses EntraPass Web may prevent use of EntraPass Web, or vice versa.

Affected platforms

exacqVision 7.4 with EntraPass 6.05.02 or newer

<br>

Symptom

By default EntraPass only allows a single connection to EntraPass Web. When exacqVision is integrated with EntraPass Web, it consumed a connection EntraPass Web. If EntraPass Web then attempts to connect, it will fail. Likewise, if EntraPass Web is connected first, exacqVision will fail to connect.

<br>

Workaround

Use only one session at a time, or contact Kantech to purchase additional licenses for web sessions.

<br>

Resolution

Fix dependent on Kantech updates to EntraPass.