Installing Exacq Web Service on 32-bit Windows fails

Description Installing the web service on 32-bit Windows fails. After installing the web service will not run, and the following error message can be found in the event viewer:The Apache service named reported the following error: >>> httpd.exe: Syntax error on line 37 of C:/Program Files/exacqVision/WebService/Apache/conf/httpd.conf: ServerRoot must be a valid directory. <br> Introduced Version… Continue reading Installing Exacq Web Service on 32-bit Windows fails