Objective Installing 32-bit Enterprise Manager on a 64-bit Ubuntu 14.04 or 16.04 Linux computer, complete the following steps: <br> Instructions Configuring a new system. <br> Setup multiarch <br> Remote Setup Ensure that X Windows can be forwarded to anyone using Putty or SSH (install gedit).Use Filezilla to transfer the debian installer to the instance.Connect using… Continue reading Installing 32-bit Enterprise Manager (EM) on 64-bit 14.04 or 16.04 Ubuntu Linux System
Tag: Installing
Installing Windows Security Essentials on Win7 based evServers
Stop exacqvision Server Service (Control Panel -> Administrative Tools ->Services -> exacqVision Server : Stop)Download Windows Security Essentials Package (mseinstall.exe, x64) from Microsoft website, and execute the installer on the target machine.Select all default options, except for the ones listed below.Do not join the program (Optional)Unselect both options below:Do not immediately scanThe system will update… Continue reading Installing Windows Security Essentials on Win7 based evServers
Bad Package Quality Error when Installing exacqVision Software on Ubuntu 11.04
Exacq recommends installing exacqVision software on Ubuntu 10.04 because of its extensive testing within the Ubuntu community and its status as a Long Term Support version. However, if you try to install exacqVision Client and exacqVision Server software version 4.5 and older, exacqVision Web Service, or Enterprise Health Manager on a Ubuntu 11.04 system, the new Ubuntu Software Center… Continue reading Bad Package Quality Error when Installing exacqVision Software on Ubuntu 11.04