ESM attempts to install postgresql even if it’s already installed

The installer for the following specific version has an option to install postgresql even if it detects a postgresql installation on the machine, however it does not work. It throws an error as it is not able to set the install path correctly. Tested Version 3.6.0 Platform Windows Steps to reproduce Install postgresql by handRun… Continue reading ESM attempts to install postgresql even if it’s already installed

Can I install Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder I’ve already purchased?

No, Kantech EntraPass cannot be installed on recorders that were purchased prior to February 9, 2016 without the CSA option. If a server was previously ordered with the CSA upgrade, you can obtain the installation and registration code from Kantech technical support or from the Kantech website registration. You may also view the FAQ page on the ExacqVision… Continue reading Can I install Onboard Kantech EntraPass Corporate Edition on an ExacqVision recorder I’ve already purchased?

Can I run a Silent Install of ExacqVision?

ExacqVision Server and Client EXE installers adhere to the normal NSIS installation options. /S runs the installer silently.for silent. Example: exacqVision_23.0.3.6_x64.exe /S /D changes the installation directory. While the default directory is recommended, you may use this option to override it to install in another directory.Example: exacqVision_23.0.3.6_x64.exe /S /D=C:\Program Files\MyCustomDirectory More information about NSIS options can… Continue reading Can I run a Silent Install of ExacqVision?

When I use a web browser to view the video from the exacqVision Web Server, do I need to install any additional software or applets?

No. The exacqVision Web Server transcodes video into a JPEG that can be viewed by any modern web browser. This allows anybody to use the Web Server without downloading or installing additional software. <br>