Description When the input is triggered on the camera, the input trigger in exacqVision client does not change state. Note: this effects Samsung SUNAPI2 cameras Steps to Reproduce Connect a switch to the cameras input trigger. In the cameraConfigure Alarm output 1 (N.O.)/Pulse/5sIn the Clientadd the camera using the Samsung pluginConfigure Trigger Input (Open)Verify trigger status Normal and… Continue reading Samsung Trigger Inputs Not working