How to set up an Association to Listen to a live view as well as Trigger a Light To notify Employees they are Being Actively Listened to

Description  If any customer is wanting to set up an event to trip when selecting 2 associations on live view to trigger a light to alert employees they are being listened in on. Product USBDIO Module: Steps to Reproduce  The task was to create a live view association as well as a trigger to turn… Continue reading How to set up an Association to Listen to a live view as well as Trigger a Light To notify Employees they are Being Actively Listened to

Samsung Trigger Inputs Not working

Description When the input is triggered on the camera, the input trigger in exacqVision client does not change state.  Note: this effects Samsung SUNAPI2 cameras Steps to Reproduce Connect a switch to the cameras input trigger. In the cameraConfigure Alarm output 1 (N.O.)/Pulse/5sIn the Clientadd the camera using the Samsung pluginConfigure Trigger Input (Open)Verify trigger status Normal and… Continue reading Samsung Trigger Inputs Not working