Connecting cameras over 100m in distance from G-Series PoE or Una recorders

ExacqVision G-Series PoE and Una recorders provide Power-over-Ethernet (PoE) ports for direct connections to cameras, rather than accessing cameras through a switched network. The TIA/EIA 568 standard provide that the maximum allowable length of a Cat5/5e or Cat6 cable is 100 meters (328 feet) for ethernet networks. To connect a camera farther than 100m away,… Continue reading Connecting cameras over 100m in distance from G-Series PoE or Una recorders