exacqVision 48- or 64-channel hybrid systems (any system with multiple Stretch capture cards) must have additional virtual memory space for the exacqVision Server software to use. To increase the virtual memory, complete the following steps: Open a command prompt with administrator privileges.Type the following command and press Enter:bcdedit.exe /set increaseuserva 2560Restart the system. If Windows… Continue reading Increasing Virtual Memory on 48- and 64-channel Hybrid exacqVision Systems