Adding the Arecont AV20476RS quad-imager camera with the ONVIF plugin may not have all (4) imager streams connect to the server

Issue: Adding the Arecont Vision ConteraIP Omni LX RS AV20476RS quad-imager IP cameras with the ONVIF plugin (onvifnvcPI) may not have all (4) imager streams connect to the server. Only (3) of the (4) imagers show as connected. Symptoms: All but one one imager on the client camera “settings” page appear functional and display live… Continue reading Adding the Arecont AV20476RS quad-imager camera with the ONVIF plugin may not have all (4) imager streams connect to the server