Illustra Pro Gen3 Motion Stops Reporting in Exacq Software

Illustra Motion stops reporting from within the Exacq Software. This has been seen on the Illustra IPS03-D12-OI03 and IPS05-D12-OI03 There is a combination of updates that need to be performed. First, upgrade the Exacq Server Software to 22.03.4 or higher Second, download Illustra Firmware version Illustra.Pro3.02.09.00.0003 and upload it to the individual cameras demonstrating the… Continue reading Illustra Pro Gen3 Motion Stops Reporting in Exacq Software