Description As a result of Cron being unavailable on Illustra Essential cameras the reboot schedule is unavailable on these devices. Cloudvue Software versions prior to 24.12.x Incorrectly display the reboot schedule. Beginning with the release of Cloudvue Software version 24.12.x the reboot schedule will no longer be displayed. Product Steps to Reproduce Results Prior to… Continue reading Reboot Schedule For Illustra Essentials C2C Removed
Tag: Illustra Essentials
New override for Dahua based OEM IP Cameras for UTC Timezone.
Issue: Adding a camera, disabling or re-enabling the camera, restarting the exacqVision server service, or rebooting the exacqVision Server, causes the server to set the camera’s timezone, for all cameras that allow it, to Coordinated Universal Time (also known as Universal Time Coordinated, UTC, UTC+0, UTC+00:00, “Z time”, or “Zulu Time”). This is preferred for… Continue reading New override for Dahua based OEM IP Cameras for UTC Timezone.
HTTPS for Illustra Essentials / Dahua cameras
To set the HTTPS mode for Illustra Essentials and any Dahua OEM cameras: Go to camera web pageEnable the HTTPS option in the Network/Connection section The camera will auto generate a self-signed certificate so that exacqVision may connect with HTTPS. Note that if the camera is in HTTPS mode and the camera’s IP address is changed,… Continue reading HTTPS for Illustra Essentials / Dahua cameras
Illustra Essentials (Gen2 cameras) motion mask not working
Motion mask configuration from the api has been updated by the firmware and now uses motion window index instead of in the motion region. For Illustra Essentials, the updated firmware supports both version 1(motion region) and version 3(motion window) types for configuration of motion mask. The supported firmware to use for Essentials Gen2 should be… Continue reading Illustra Essentials (Gen2 cameras) motion mask not working
Illustra Essentials low quality in MJPEG
Description When connecting to some essentials camaera’s OEM’ed by Dahua, the customer can put the camera in a mode that shows jpeg in a low quality and the quality slider has no apparent effect. To reproduce Workaround