Affected platforms Illustra cameras running the exacqVision Edge application in non-DHCP environments <br> Description In a non-DHCP environment, a factory default Illustra camera will acquire a known IP address of 192.168.1.168. Follow these steps to assign the desired IP address to the edge camera:- Connect the Edge camera to the network. <br>