Some Illustra Cameras will Connect but then Disconnect After 1 Minute

Issue Some Illustra models, specifically ISL02B1BNWIY, will initially connect, but then disconnect after 1 minute.   <br> Workaround Downgrade to 20.03.5 server.Specify #transport=rtspSpecify #transport=udp <br> Resolution   Fixed in exacqVision Server 20.03.124   <br> Version Affected exacqVision Server 20.03.6   <br> Version Fixed exacqVision Server 20.03.124