Dell Notice: Updating Dell Hard Drive Firmware

Navigate to the following link. How to Update PowerEdge Firmware Using iDRAC9. Select the triangle next to HDD or SSD a. (example R660, US) Dell Drivers and Downloads for R660Click Category and select “SAS Drive” or “Solid-State Storage,” in the list find the drive (or drives) you would like to update. b. There are a lot of drives… Continue reading Dell Notice: Updating Dell Hard Drive Firmware

Using iDRAC on X-Series NVRs

What is iDRAC? Integrated Dell Remote Access Controller (iDRAC) is a proprietary technology that allows IT administrators to remotely manage and monitor Dell-built servers. This includes software and hardware components. The Exacq X-Series NVRs include iDRAC micro ports on the front of the system and iDRAC network interfaces on the back. The location of these… Continue reading Using iDRAC on X-Series NVRs