This is because that control should be provided by the encoder and the PTZ plugin is not installed. <br>
Tag: Hybrid Systems
exacqVision Q-Series IP and Hybrid Systems
Can exacqVision Hybrid Systems use MPEG-4 Simple Profile?
Yes. eDVR systems use MPEG-4 Advanced Simple Profile by default, and sDVR systems use H.264 by default. To configure the system, complete the following steps for your system type. <br> eDVR Systems Stop the exacqVision Server in Service Control Manager or by running sudo /etc/init.d/edvrserver stop.Open c:\windows\XDVAPI.ini in Notepad or run sudo nano /usr/local/xdvapi/etc/XDVAPI.ini.Add MPEG… Continue reading Can exacqVision Hybrid Systems use MPEG-4 Simple Profile?