Title HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers Description exacqVision hybrid servers do not natively support HD analog cameras too include HD-TVI, HD-SDI, HD-CVI and AHD Product exacqVision Server Solution An encoder which supports HD analog will be required to connect an HD analog camera to an exacqVision… Continue reading HD Analog Cameras are not Natively Supported on exacqVision Hybrid Servers
Tag: Hybrid
exacqVision A-Series Hybrid F2A
Z Series 4U Hybrid NVR Series Quick Start Guide
Z Series 2U NVR Series Quick Start Guide
A-Series 2UA/F2A IP Server Quick Start Guide
A-Series Hybrid/IPS Desktop Quick Start Guide
A Series 4U Hybrid NVR Series Quick Start Guide
exacqVision Z-Series Hybrid & IP Network Video Recorders
exacqVision A-Series Hybrid and IP Network Video Recorders
What types of microphones are compatible with the ExacqVision Hybrid NVR?
When using the audio input terminals on the rear of an ExacqVision Hybrid NVR, you will need a microphone with a a pre-amplifier capable of producing a line level output that can be connected directly to the ExacqVision audio terminal inputs. If using a mic level output microphone, you will need a mic pre-amp to… Continue reading What types of microphones are compatible with the ExacqVision Hybrid NVR?