Let’s Encrypt Auto Renewal Fails with Redirect Enabled

Title Let’s Encrypt Auto Renewal Fails with Redirect Enabled Description  If you are using Let’s Encrypt with HTTPS Redirect enabled the auto renewal can provide random internal IP addresses that fail to renew. Product  WebService 20.06.2.0 to current 22.03.02.0 Steps to Reproduce  Engineering was able to Reproduce this behavior and determined that Redirect should be… Continue reading Let’s Encrypt Auto Renewal Fails with Redirect Enabled

exacqVision Web Server HTTP Policy “Redirect to HTTP” Broken

Description  HTTP to HTTPS redirect implementation is broken and always supplies and internal IP address for the redirect, leading to any and all redirect from outside of the local network to fail.   Product  Steps to Reproduce  Expected Results  HTTP requests are redirected to HTTPS   Actual Results  Fails to connect   Solution Update exacqVision… Continue reading exacqVision Web Server HTTP Policy “Redirect to HTTP” Broken

Redirecting HTTP to HTTPS with Web Sevice 9.0 – 19.06

NOTE: This document does not apply to Web Service versions 19.09 and higher. Best Practice is to use the latest version of Web Service available. The way the web service handles HTTP requests when HTTPS is configured can be controlled with the webserver.tls.httpPolicy key: Open the following file in a text editor: Windows: C:\ProgramData\Webservice\conf\wfe.jsonLinux: /etc/webservice/wfe.json Add the… Continue reading Redirecting HTTP to HTTPS with Web Sevice 9.0 – 19.06