Code Description Definition Exacq Tips Informational 100 Continue Server received request, client should continue. 101 Switching Protocols Response to upgrade header 102 Processing Server processing received request. 103 Early Hints Used with link header.Allows browser to preload resources. Successful 200 OK Standard response for successful request.Meaning varies based on method (GET, POST, etc). 201 Created… Continue reading HTTP Response Code Reference
Tag: HTTP
exacqVision Web Server HTTP Policy “Redirect to HTTP” Broken
Description HTTP to HTTPS redirect implementation is broken and always supplies and internal IP address for the redirect, leading to any and all redirect from outside of the local network to fail. Product Steps to Reproduce Expected Results HTTP requests are redirected to HTTPS Actual Results Fails to connect Solution Update exacqVision… Continue reading exacqVision Web Server HTTP Policy “Redirect to HTTP” Broken
Green Lock and Gear Icons in the exacqVision Client
Description A green icon indicates a secure (HTTPS) connection is being used for either or both the configuration connection to the device and/or the video stream. Product exacqVision Client Solution The green lock and gear icons are used as a visual indicators of the connection protocol being used by the camera. They can be found… Continue reading Green Lock and Gear Icons in the exacqVision Client
How to change web service ports
There are two ways to modify the ports used by the Web Service: It is recommended to use the configuration interface, whenever possible. However, it is possible that you must hand edit the configuration in cases where the Web Service cannot start (for example, if there is a port conflict). This article provides instructions for… Continue reading How to change web service ports