To create a shutdown hot key on a Linux ExacqVision system, complete the following steps: Ubuntu 20.04 & 18.04 These systems are already configured to use CTRL+ALT+DEL to pop up a dialogue with a shutdown option. Once the dialogue opens the system will shutdown if no further user interaction occurs. Ubuntu 16.04 and earlier This… Continue reading Creating a Shutdown Hot Key in Linux